Post Go back to editing

AD5781 hardware and software setup

Dear Friends:

I plan to use AD5781 for my project. I have three questions: 1) if I plan to set the LDAC permanently low, should I use a resistor between LDAC and GND? 2) if I do not plan to use CLR, can this pin be disconnected? 3) if I want the a predetermined Vout right after the chip goes to normal mode, I should load DAC register before the control register, am I right?

Thank you

Parents
  • Hi Peter,

    1)Write DAC register values 

    2) pull LDAC pin to low or issue software LDAC (always low is also an option, please refer to page 20 of the datasheet for complete details)

    3) set to normal mode

    By doing this, you should expect that the output goes to the equivalent output voltage of the DAC register sent in step 1.

    Do you mean it's difficult to install LFCSP packages on boards? I do agree that it is challenging, but you may want to check this thread with a video link on how to hand solder a LFCSP device. May I also know which 24-lead LFCSP DAC you are referring to?

    Cheers,

    Ivan

Reply
  • Hi Peter,

    1)Write DAC register values 

    2) pull LDAC pin to low or issue software LDAC (always low is also an option, please refer to page 20 of the datasheet for complete details)

    3) set to normal mode

    By doing this, you should expect that the output goes to the equivalent output voltage of the DAC register sent in step 1.

    Do you mean it's difficult to install LFCSP packages on boards? I do agree that it is challenging, but you may want to check this thread with a video link on how to hand solder a LFCSP device. May I also know which 24-lead LFCSP DAC you are referring to?

    Cheers,

    Ivan

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.