Can the Rofs pin of the AD5556 be left unconnected when used in unipolar two-quadrant mode? It appears that this would increase the feedback resistance from 5kΩ to 10kΩ. Would this then also increase the output range from 0V - Vref to 0V to 2Vref?
Can the Rofs pin of the AD5556 be left unconnected when used in unipolar two-quadrant mode? It appears that this would increase the feedback resistance from 5kΩ to 10kΩ. Would this then also increase the output range from 0V - Vref to 0V to 2Vref?
Hi Ivan,
Thank you for responding.
I'm going to connect the parallel data inputs to the databus of a non-volatile memory and modify the effective reference input to 'compensate' the contents of the NVM. The effective reference input ended up being -1.5V, so I was hoping to find a way to 'boost' the output to increase the range without adding additional components and decreasing the reliability of the system.
Thanks,
James
Hi Ivan,
Thank you for responding.
I'm going to connect the parallel data inputs to the databus of a non-volatile memory and modify the effective reference input to 'compensate' the contents of the NVM. The effective reference input ended up being -1.5V, so I was hoping to find a way to 'boost' the output to increase the range without adding additional components and decreasing the reliability of the system.
Thanks,
James