Post Go back to editing

DAC update rate

I plan to use AD5672, but the update rate is not described in parametric search and AD5672 data sheet.

 

DAC Parametric Search with update rate

http://www.analog.com/en/parametricsearch/10933#/p4910=Precision%20DAC&d=sel|0|4527|s8|4910|7|165|4458|3899|4737|4129|3970|s3|s5


How do I think the update rate?
(compare the slew rate and input shift register time (t1 x 24bit) and choose the longer time?)

Would you tell me the AD5672 update rate?

Parents
  •  

    Thank you for your answer.

    Your advice is very useful to me.

    I have additional questions.

     

    Q1.

    It is described at AD5791 datasheet

            T17 : /SYNC rising edge to output response time(/LDAC tied low) (datasheet Rev.D table 4)

            Tsettle(Output Voltage Settling Time) : Output Voltage Settling Time is the amount of time it takes for the output voltage to settle to specified level for a specified change in voltage.(datasheet Rev.D P17)

     

    It is described at AD5672R datasheet

            T17 : (There is no equivalent parameter.)

            Tsettle(Output Voltage Settling Time) : The output Voltage Settling Time is the amount of time it takes for the output of a DAC to settle to a specified level for a 1/4 to 3/4 full-scale input change and is measured from the rising edge of /SYNC.(datasheet Rev.B P22)

     

    Does it means that Tsettle(@AD5672R) = T17 + Tsettle (@AD5791) ?

     

    Q2.

    It takes settling time about 140+[us] from AD5672R/Figure41.

    What is the start point the settling time?

    Would you tell me the difference between AD5672R/Figure 41 and AD5672R/Figure 51?

Reply
  •  

    Thank you for your answer.

    Your advice is very useful to me.

    I have additional questions.

     

    Q1.

    It is described at AD5791 datasheet

            T17 : /SYNC rising edge to output response time(/LDAC tied low) (datasheet Rev.D table 4)

            Tsettle(Output Voltage Settling Time) : Output Voltage Settling Time is the amount of time it takes for the output voltage to settle to specified level for a specified change in voltage.(datasheet Rev.D P17)

     

    It is described at AD5672R datasheet

            T17 : (There is no equivalent parameter.)

            Tsettle(Output Voltage Settling Time) : The output Voltage Settling Time is the amount of time it takes for the output of a DAC to settle to a specified level for a 1/4 to 3/4 full-scale input change and is measured from the rising edge of /SYNC.(datasheet Rev.B P22)

     

    Does it means that Tsettle(@AD5672R) = T17 + Tsettle (@AD5791) ?

     

    Q2.

    It takes settling time about 140+[us] from AD5672R/Figure41.

    What is the start point the settling time?

    Would you tell me the difference between AD5672R/Figure 41 and AD5672R/Figure 51?

Children
No Data