Post Go back to editing

Spice model of AD5144

Thread Summary

The user inquired about the AD5144 SPICE model, confirming if the AD5140 model is applicable, understanding the independent and pot modes, and the possibility of modifying the model for 100k ohms. The support engineer confirmed the AD5140 model is correct for AD5144, explained that the 9-pin is for independent control allowing separate programming of Raw and Rbw, and advised against altering the model without SPICE experience.
AI Generated Content

Hello,

I have some questions about the spice model of AD5144.

(1) I downloaded the spice model from ADI WEB site. The file name is AD5144_10k.cir. But the first line of the description of the model is AD5140 SPICE MACROMODEL. Is this file correct spice model of AD5144?

(2) According to the description of the model, 9pin is for independent control. Could you please advise me the independent mode and pot mode?

(3) The model is for 10k ohms. Can I change the model to 100k ohms? If yes, how can I change it?

Best Regards,

Akira

Parents Reply Children
No Data