Post Go back to editing

How do I use ACE software to transfer digital quantity to analog quantity continuously in AD5696

I bought the AD5696 evaluation board  EVAL-AD5686RSDZ and control board EVAL-SDP-CS1Z

,I can use ACE software to convert a digital quantity into analog quantity manually, but I need to convert digital quantity into analog quantity continuously and automatically, What should I do?

Parents
  • Hi,

    As there are only 6 pins connected to YRDKRL78G13, you need to manually configure A1, A0, RSTSEL, and GAIN pins of the device on the EVAL-AD5696RSDZ or, you can also connect it to YRDKRL78G13 which means you have to add pin definitions on the files.

    You also need to supply VIO externally, VDD can be supplied externally or use the PWRSEL of the evaluation board to select the supply.

    Since you are using the exact YRDKRL78G13, there's no need to reconfigure the peripherals and pin assignments as it is already in the drivers. You just need to use the defined functions as stated in the no OS wiki.

     

    Cheers,

    Ivan

Reply
  • Hi,

    As there are only 6 pins connected to YRDKRL78G13, you need to manually configure A1, A0, RSTSEL, and GAIN pins of the device on the EVAL-AD5696RSDZ or, you can also connect it to YRDKRL78G13 which means you have to add pin definitions on the files.

    You also need to supply VIO externally, VDD can be supplied externally or use the PWRSEL of the evaluation board to select the supply.

    Since you are using the exact YRDKRL78G13, there's no need to reconfigure the peripherals and pin assignments as it is already in the drivers. You just need to use the defined functions as stated in the no OS wiki.

     

    Cheers,

    Ivan

Children
No Data