Post Go back to editing

AD5686R operation with GAIN=2

Hi,

Request your help to understand why the gain error is improving with Gain=2 compared to Gain=1?

Also with Vref=2.5V & Gain=2, what should be the minimum VDD requirement to get output of 3V?

I have seen Vref+1.5 as the minimum power supply required, is it still valid even if the max output needed is 3V?

Thanks

Shihab.

  • Hi Shihab,

    Apologies for the late response. What you observe is possible as the resistors with gain of 1 are not perfectly matched. For your second question, you could add around 10mV headroom above 3V output as the minimum Vdd.

    And for the third one, let me ask around to clearly answer that question and will get back to you. Hope that helps!

    Cheers,

    Ivan