Post Go back to editing

AD7847

Timing about AD7847:

In the AD7847 datasheet, I got the truth table and write timing diagram as below:

  

I have confusions:

(1) from the truth table, I think that both CS and WR rising edge can latch data into the DAC.

(2) But from the timing diagram, it seems that CS has to be wider than WR.

So I am not sure what will happen if the timing is below:

or 

or 

I think all of the timings above will work if I follow the truth table.

But from the timing diagram, t1 and t2 is 0(min), then all the above timings I described can not work.

So could you please give me some guidance about the timing requirement? 

Looking forward to your reply.

Thank you very much!

BR//Maggie