Does any one use the AD5592r sequence conversion mode (or so called the burst mode)? I am experiencing some issues when use the sequence conversion mode. In general, it works fine but once a while, the AD5592r will send two consecutive channel 1 ADC value out.
for example:
The following is the correct ADC values with the correct channel inex.
| 0207 | 11C4 | 2197 | 31EB | 41D4 | 519F | 61DF | 71BC |
But once a while the first channel ADC will be sent twice miss the last channel ADC value
| 0207 | 0208 | 11C4 | 2196 | 31EB | 41D3 | 519E | 61DF |
The failure rate is around 0.5%. There is no pattern. it is purely random.
I will appreciate if any one has any answer or solution.
Marc