The datasheet states that the single supply range is from +9V to +33V, but oddly enough the dual supply range does not start from +/-4.5V (as expected) but from a much higher +/-9V. Now, I suspect that this must have something to do with a requirement for a voltage differences between the digital and analog supply, which needs to have a certain "spacing" for the dual supply case. Would it be still possible to supply the AD5292 from +/-5V if,a) GND was tied to -5V, b)Vlogic to 0V and c) the digital signals were level shifted from 0V/3.3V to -5V/0V? This would correspond to a "single supply" voltage of +10V with regards to the common negative rail of -5V. Would this be a work around if +/-5V was the only voltage level that I could supply?