Post Go back to editing

AD5253 Reading sequence

Thread Summary

The user inquired if NOP commands are required when reading from EEMEM0-EEMEM3 in a direct read sequence. The final answer clarifies that NOP is only necessary after using Command 1, not for direct reads from EEMEM. The evaluation board GUI sends NOP after write and read operations in the 'UPDATE SINGLE' (READ) command, but not in 'STORE' or 'UPDATE SINGLE with WRITE'.
AI Generated Content

Hi

I have a quetion about NOP in direct read sequence.

About D/S discription (below), Reading user data directly from EEMEM dose not require a similar NOP command execution. 

but user data is only EEMEM4-EEMEM15

Are EEMEM0-EEMEM3 required NOP command in read sequence?

Best regards 

Thank you very much.

Parents Reply Children
No Data