Post Go back to editing

How to use the "Load Regulation" parameter correctly? AD5421

How to use the "Load Regulation" parameter correctly?
It seems to me that load regulation is a decrease in the output voltage when the load current increases by 1 m A. If so, can I assume that with a load current of 20 mA on the REGout pin and with a configured output voltage of 12V on the REGout pin, as a result of the voltage drop, I will get this output voltage by calculating this formula which I made for the REGout pin: V(REGout)=12V-(20mA*8mV/mA)= 11840 mV= 11.84 V .

https://www.analog.com/media/en/technical-documentation/data-sheets/AD5421.pdf

Did I understand Correctly and calculate the final voltage for the pin regout?

Parents Reply Children