Post Go back to editing

AD5693 I2C pin fall time requirement

Hi.

We are using DA-converter AD5694 in out design.

I2C bus speed is close to 400kHz i.e it is used in fast mode. I2C specification state the same requirement for signal fall time as is stated in AD5694 data (table 4, page 4)

Requirement for the fall time is 6.54ns when V_LOGIC is 1.8V.

Fall (and rise) is measured between 30% and 70% level according to I2C specification

https://www.nxp.com/docs/en/user-guide/UM10204.pdf

Questions :

Signal fall time measured from design is close to 6ns, so it is a bit faster than required 6.54ns.

 - Is fall time too fast for the AD5693 I2C bus interface as stated in data (and I2C specification)?

 - Can you define component specific value for signal fall time which is safe to use without compromise functionality?

Thank you for your reply in advance!

  • Hi,

    Are you using pull-up resistors from SCL, SDA lines to the Vlogic supply? 

    You can basically increase the resistor value just a bit in order to meet the minimum requirement in the data sheet.

    Cheers,

    Ivan

  • Hi,

    Thank you for reply.

    SCL,SDA lines pull-up resistors are connected to Vlogic supply. Resistor value is 1k, same value for both lines. 

    I2C bus master has configurable drive strength and is set to minimum 2mA value. with 1k pull-up, fall time is still a bit too fast as specified for AD5693/I2C specification.

    But has other I2C nodes as well and they all have differences in drive strength. However there will be some margins to  increase pull-up strength to restrict fall time.

    So answer to original questions "does AD5693 have component specific fall/rise time value" is no, and we have to follow I2C specification?

    Other I2C node ICs we are using will define component specific value for fall/rise time.     

    Br,

    Sami

  • Hi ,

    Yes, no specific resistor value required as long as you meet the requirements in AD5693 timing specifications.

    Curious question, what's the i2c bus master you are using? looks like it has a built in pull-up resistor or constant current source, if this is the case, not sure why would you need additional 1k pull-up. is my understanding correct?

    Cheers,

    Ivan

More Content

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.