AD5522 FN-MI mode with internal Rsense

Hi, 

I would like to use AD5522 with no force voltage (HiZ) - measure current mode.

Would you show the diagram of the connection the inernal Rsense to the measurement pins?

When CH EN bit is disabled, SW5 is opened and SW2 is closed. When SW5 is opened, the no pins could connect to current inamps.

(refer to the discription of CH EN bit of Table 26 and Figure1)

It's ok the connection to the external Rsense.

Thanks,