I would like to use an LT1010 output buffer:
...with the LTC2757 DAC:
The LT1007 as shown in the buffer schematic will be substituted for the LT1468 shown in the DAC schematic. My questions are:
1. Where should I connect the DAC's Rfb input? Should it be connected to Vout on the buffer?
2. Should the 27pF cap shown in the DAC schematic stay connected between Rfb and Iout1, or should it be connected somewhere else?
Thanks,
Justin
Edit Notes
added a signature[edited by: justinis at 4:12 PM (GMT 0) on 6 May 2019]