Post Go back to editing

First time using the LTC2634 (or any DAC) with Arduino - just need assurance that connections are correct

Dear Precision DAC Forum,

     I'm quite new to data converter use, and I've designed a circuit where an Arduino Pro Micro PCB is connected to your LTC2634-HZ10 DAC. I was hoping you could look at the schematic and tell me if the connections are correct.

My principal concern is that the MISO and MOSI of the Pro Micro are connected to the proper pins of the LTC2634. If the answer is "that depends, provide more details" then I will happily do so.

Many thanks,

Chris