Post Go back to editing

LTC1668 Gain Error

In a circuit with a LTC1668 driving a differential buffer stage, and using precision (0.1%) resistors, I'm seeing an output gain error of -4% (there's small variation from unit to unit, but the error is always close to -4%).  I've seen the same error across three different revisions of the PCB, on 15 different individual assemblies, both hand built and machine built.

The error isn't a problem - I can very easily compensate for it - but I'd like to get to the bottom of its source.

This is the buffer stage:

Not shown is the LTC1668 reference input, which is driven externally by a LTC6655-4.096 (Vref) through a 0.1% 3.32k resistor (Rref).

The buffer stage is the same topology as the buffer in figure 7 of the LTC1668 data sheet, but the component values are different.

The amplifier is an ADA4637-1.

Given all that, with a DAC code of D:

The factor of 8 is taken from the LTC1668 datasheet, the rest is from basic circuit analysis.  RV = 49.9R, RI = 1k, RF = 6.81k at the moment, but the exact values aren't important.  I've used a couple of values for RF during testing, but the error is always -4%.

Anne know what the explanation is, or seen the same issue?

More Content

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.