AD5755-1 voltage and current mode at the same time?

Hello

AD5755-1 has 4 channels and supports both voltage output and current output mode.

Does anyone know if it's possible to use both modes at the same time? For example use 3 channels in voltage output mode and 1 in current mode? Or 2 channels in voltage mode and 2 in current.

Thank you

    •  Analog Employees 
    on Sep 7, 2016 4:30 PM

    Hi,

    Yes each channel can be configured independently using the DAC control register.  So any combination of channels can be assigned as you've outlined. 

    Regards,

    Michael