Article For MAX5054B, What is the minimum value of VIL for logical input? What's the typical value and temperature trend of these values?

1.The 0.8V value given in the EC table is sufficient for design, since this is the maximum allowed input signal voltage that is guaranteed to be recognized as a logic low input. 
2.These EC table numbers are guaranteed over -40 to 125 deg C.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.