Article Can I parallel multiple DAC output ports of the MAX11300 to increase current drive capability?

Each DAC-configured PIXI port has a 25mA (sink or source) output drive capability, with a current limiting feature of 50mA. If the application needs to drive a higher output current (for example 50mA), then two-DAC ports can be used in parallel to the external load.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.