Article Can I have the MAX11300 ports configured as ADCs with different I/O voltage ranges?

Yes—you can have up to 20 ports configured as single-ended ADCs or 10 differential ADC configurations; each input can be configured as one of four voltage ranges from 0 to 10V, -5V to +5V, -10V to 0, or 0 to 2.5V.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.