Article AD5301 Signal Accuracy and Absolute Error

Question

I am using the AD5301BRM. THe datasheet states the accuracy is 1LSB.

1. Is such accuracy correct for AD5301BRM?

Answer

1. You should indeed get a result of 1 LSB if you are measuring correctly.
Did you notice "note 4" at the bottom of page 2 of the datasheet
"4 Linearity is tested using a reduced code range: AD5301 (Code 7 to 250);".
Since the AD5301 uses its power supply as the reference , using this slightly
restricted range removes the
deadband near to ground and Vdd; we have to do this because the output buffer
can never reach the full 0 and Vdd rails : "rail to rail" really means "almost
rail to rail".
Results will also be worse if you are driving less than 2 Kohms at the output.

The ideal measurement would be between codes 7 and 250 with a clean, properly
decoupled voltage reference used as the power supply. Figure 31 in the
datasheet shows an example of this.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.