MAX5214GUA+: FAQ

  • Created
Was this helpful?
  • Confusion of MAX5214 write command

    Q: In Table1 of MAX5214's datasheet, the 'Write Through' function requires to set D15:14 to 0:1. But in Table1, its D15:14 is not comply with Table1, it this one TYPO? A: No, it is not one…
  • Why MAX5214 has no output?

    Q: Customer is using MAX5214, the schematic looks correct, but there is on output. What is the reason? Below is the schematic Below is the waveform: A: According to schematic, it looks there…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.