1. First, please make sure that you can get an acknowledge bit from the device when you are sending the slave address byte. This ensures that you are able to start communicating with MAX5116.
2. If you are writing to all four non-volatile register of DAC0 to DAC3 consecutively, please make sure to leave a 15ms delay in between each write. Do not repeatedly send in the write command during the delay. 15ms is the maximum "Write NV Register Busy Time" and the busy time begins from the initiation of the stop pulse.