1.The 0.8V value given in the EC table is sufficient for design, since this is the maximum allowed input signal voltage that is guaranteed to be recognized as a logic low input.
2.These EC table numbers are guaranteed over -40 to 125 deg C.
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
1.The 0.8V value given in the EC table is sufficient for design, since this is the maximum allowed input signal voltage that is guaranteed to be recognized as a logic low input.
2.These EC table numbers are guaranteed over -40 to 125 deg C.