Q
I am looking at using the DEMO-AD5700D2Z kit (Complete 4 mA to 20 mA LoopPowered Field Instrument with HART Interface) and want a low cost development
environment for modifying the sample code provided. Please can you advise which
IDE I should use as the list on your pages doesn't seem to include the M3
products.
A
Any tool supporting SWD and Cortex M3 can be used for the development with ourCortex M3 products including the ADuCM360 microcontroller used on
DEMO-AD5700D2Z kit
There are several free IDEs that you could use, for example:
emIDE : www.emide.org/
Eclipse: www.eclipse.org/
Other useful resources:
ADuCM360 Development system webpage:
http://www.analog.com/en/processors-dsp/analog-microcontrollers/aducm360/product
s/EVAL-ADUCM360/eb.html
We provide code limited evaluation versions of IAR and Keil with our Cortex M3
based ADuCM360 Developments kits:
http://wwwp.analog.com/en/evaluation/eval-aduc-cable1z/MicroConverter_Developmen
t_Tools/fca.html#cortexM3
Links to IAR and Keil:
http://www.iar.com/
http://www.keil.com/arm/mdk.asp