AD5383: FAQ

  • Created
  • Updated
Was this helpful?
  • AD5383: Pin connections

    Question A. SER/PAR' pin should it be connected to DGND? B. Where should I connect REF_GND and REFOUT/REFIN pins? C. FIFO_EN pin should it be connected to DGND? D. Where should I connect MON_OUT & mON_IN…
  • AD5383-5 maximum current that can be supplied by each voltage output?

    Q I would like to ask if the short circuit current of 40mA is the maximum current that the voltage output can provide or if it is just the 1mA marked as load current. A The specified load for each…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.