Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question

Difference between AD7656 and AD7656-1

Q: What are the similarities and differences between AD7656 and AD7656-1?

A:

  • The AD7656-1 is a pin to pin and software compatible upgrade to the AD7656.
  • The AD7656-1 has reduced decoupling requirements and reduced bill of materials cost compared with the AD7656.
  • Both parts contain low noise, wide bandwidth, track-and-hold amplifiers but differ in full power bandwidth. The AD7656 can handle input frequencies up to 12 MHz, the AD7656-1 can handle up to 4.5 MHz.
  • Functionality-wise, the only difference is that the AD7656 can work with a 2.5V or 3V reference whereas the AD7656-1 can only accept a 2.5V reference.
  • There are AC/DC specification differences that could affect calibration routines – please refer to the datasheet specification table for more information.
Comments
Anonymous
Parents Comment Children
Related