Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question

ADAS3023 - power supply sequencing

Q: What is the correct power supply sequence for the ADAS3023 to operate properly?

 

A: The ADAS3023 requires these five supplies: AVDD = +5V, DVDD = + 5V, VDDH = + 15V, VSSH = - 15V, and VIO = 1.8V to 5V. The user must bring up the ADAS3023 power supplies in the following sequence in order to operate it normally:

1. VIO

2. VDDH

3. VSSH

4. DVDD

5. AVDD

6. REFx

In order to operate the ADAS3023 from a + 5V single supply, the user would need to generate the required +/-15V high voltage supplies using one of our switching converters such as the ADP1613/14 in SEPIC-Cuk topology. Refer to CN-201 for complete information on this test setup.

Comments
Anonymous
Parents Comment Children
No Data
Related