Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question

AD2S1210: FAQs

Is it possible to operate two AD2S1210 converters with one resolver?
 

 

It is possible to operate two AD2S1210 covnerters with one resolver however
proper synchronisation procedure must be followed.
 
1. Both devices must be clocked with the same signal from the same clock source
(CLKIN input)
2. After initial configuration of the AD2S1210s the Software Reset command
should be issued to both devices simultaneously.
 
If this recommendation is met both devices are synchronised hence operation
with one sensor is allowed. In case of  using two RDC chips which are not
succesfully synchronised user may experience faults and incorrect output data
from one device.
 

 

 



 

Comments
Anonymous
Related