Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question

AD2S80: Accuracy vs. temperature FAQs

What is the difference between the AD2S80ABD and the AD2S80ASD ?

Is the ASD just more classified than the ABD according to accuracy/temperature?
I mean, has the ASD and the ABD the same accuracy of 4 arcmin between -40?C
and  85?C ? Or does the ASD type have a accuracy of 8arcmin over the whole
range ?

I will need a AD2S80 that has an accuracy of 4arcmin between -20?C and  75?C.

 

All the parts have been tested over the full temperature range. And the
variation in accuracy is never bigger than 1 arc min.
Therefore for a temp range between –20 and +75degC you have the BD (Industrial)
and TD (military) with an accuracy of ±4 + 1 arc min (the +1 means that it can
change until 1 arc min more over the range) and the UD (military) with an
accuracy of ±2 + 1 arc min.
The SD you mention has a ±8 + 1 arc min accuracy.

Comments
Anonymous
Related