Q
Would the AD7280 work with 3 cells if a cell has:
Nominal Voltage: 3.7V
Cut-Off Voltage: 2.7V
Continuos Current: 150.0A
3*2.7V=8.1V – which is 100mV above the 8V min – and this in general speaking
(+-10%)
A
Yes, as soon as minimum voltage is above the AD7280 VDD min specification the
part will work.