The MAX11625 is not designed to support daisy-chain mode. The DIN pin is used for device setup and configuration, not daisy-chain purpose
MAX11625
Production
The MAX11618–MAX11621/MAX11624/MAX11625 are serial 10-bit analog-to-digital converters (ADCs) with an internal reference. These devices feature on-chip...
Datasheet
MAX11625 on Analog.com
TOOLS-MISC
Obsolete
The Link Port Cable allows you to link an EZ-KIT Lite to another EZ-KIT Lite.
TOOLS-MISC on Analog.com
The MAX11625 is not designed to support daisy-chain mode. The DIN pin is used for device setup and configuration, not daisy-chain purpose