If the MAX1115X or MAX1116X EVKIT is put in shutdown using the GUI and then a data read is started it will pull the part out of shutdown and remain as such without unchecking the shutdown box on the GUI. The user must uncheck and recheck the shutdown box to put the device back into the state, otherwise the MAX1115x or MAX1116X IC will remain in active mode.