Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question.
I would like to calculate the total temp. Coefficient of this component. If i use the RFB as the feedback resistor of the external Amp. and connect an external Ref. what is the total temp. Coefficient with respect to the following Spec's: 1. Gain Temp. Coeff.: 5ppm/C 2. Input Res. Temp. Coeff.: -300ppm/C
Provided that the Vref is a low impedance source, the effect of the absolute change in i/p resistance will not affect the gain tempco of the device. Therefore you should use a low impedance ref source and use the gain temp.co-eff of 5ppm/degC as your reference.