Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question.
I have a question to the timing of AD7655 in master-mode. Does the following operational sequence function? MASTER MODE: In the first run an low-impulse on the CNVST line must take place to start the automatic conversions. 'Start': - wait until BUSY (or EOC) goes high - store the value of the channel A - change A/B - wait until EOC goes high - store the value of the channel B - change A/B Goto 'Start' Only does one impulse on the CNVST line have to take place, to start all other conversions?
In NORMAL mode you need to apply a low going pulse on CONVST\ for EACH conversion in e frequency of CONVST is equal to the conversion frequency. The internal clock inside the AD7655 is only used to take the conversion from start to finish but the user has to start each conversion with a low going pulse. The CONVST\ signal does not need to be a short pulse. It can have a duty cycle of 50%. It is only the falling edge that is important. In IMPULSE mode you only need to apply the first low going edge on CONVST\. If you hold CONVST\ low after that, a new conversion will start each time the BUSY line goes low. This will result in an overall conversion rate of around 888kSPS, but this is subject to quite a wide tolerance since the frequency of the internal clock is not very precise.