Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question

AD7656: FAQs

My question is the same, but for two different devices, AD974 and AD7656. I
want an input range of at least +/-5V, and from what I understand from the
datasheets, I can use both of the devices as single ended, i.e. I can use the
four inputs on the AD974 for four different signals and still have an input
range of +/-10V and the same for the AD7656, I can use the six inputs for six
different signals and still have an input range of +/-5V.

so my question is quite simple, can I use the devices with bipolar inputs and
still get an input range of +/-5V respectively +/- 10V??

 

To answer your question yes you can use the devices with bipolar inputs, AD974
only have bipolar +/-10V input range, input range for the AD7656 is Vin = +/-5V
or +/-10V depending on the range pin referenced to ground. NB: The supplies Vdd
and Vss must always greater or equal to the input swing.

Comments
Anonymous
Related