Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question

AD7691: Vref

Question on AD7691: What should be Vref to convert of the maximal number of
bits a difference between two signals which a little from each other differ?
For example, Vin + = 4,5V, Vin-= 4,49V.

 

As the absolute input range max is =Vref and your signal max is = 4.5volts,
then you can't use a lower ref value less than 4.5volts. So assuming you are
using supplies of 5volts, you should take your Vref from your 5volt supply and
use a common mode of 2.5volts Vref/2.

The main requirement of Vref is that it should be a low impedance source with
recommended decoupling to act as a reservoir of charge.

Driving the part differentially is important in order to get performance.

Comments
Anonymous
Related