Q
I got last week the evaluation board for the AD7994. I installed the software
and connected the board via the USB to a Windows7 (64-bit) PC. The OS complains
about the USB device driver. So I can't use the board and the software so far.
Could you provide me a driver, or do you have any suggestion to make the HW/SW
running.
A
You probably received a CD before we updated the installation SW with 64-bit
drivers. The software version that is available on the web is supposed to
operate on 64-bit operating systems. This particular version was tested on
Windows XP and Windows 7 in December 2013. I suggest you download this version
and check whether you can get the hardware/software running this time.
http://www.analog.com/static/imported-files/eval_boards/AD7993_AD7994_Evaluation
_Software.zip