Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question

AD7927: Vdrive voltage

In page 3 of the datasheet, the specification indicates that the analog input
can be 0~2*REFin. The condition is AVDD/VDRIVE=4.75~5.25V. It requires both
AVDD and VDRIVE to be 5V. However, in the datasheet, it says the Vdrive can be
3V to interface 3V MCU even at AVDD = 5V. Whether the VDRIVE needs to be 5V as
well when he choose 0~2*REFin input range. I used 3V MCU in the system.

 

There is no need to use the same voltage value for both supplies. The AVDD
should be tied to 4.75-5.25 V but VDRIVE pin can be connected to lower voltage,
for example 3 V.

Attachments:
Comments
Anonymous
Related