Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question

Common-mode range requirement for the AD7961?

What is the common-mode range requirement for the AD7961?

 

The AD7961 common-mode input voltage (VCM) range is half of the external
reference voltage used. For example, if the 5V external reference voltage is
used, the VCM would be 2.5V in this case.

Comments
Anonymous
Related