Q
I need support about the ad7980-ep ADC, when I read the technical datasheet, Ihave two values about the absolute input voltage.
On page 3, there is this value Vref + 0.1V
But on page 6, there is the absolute maximum rating table, here the value is
+0.3V.
I would like to know which value is the maximum input voltage for the AD7980
chip to choose the right protection scheme.
A
The maximum allowed from a protection standpoint is 0.3V. Anything above thatcould result in damage of AD7980-EP.