Q
I got last week the evaluation board for the AD7994. I installed the software
and connected the board via the USB to a Windows7 (64-bit) PC. The OS complains
about the USB device driver. So I can't use the board and the software so far.
Could you provide me a driver, or do you have any suggestion to make the HW/SW
running.
A
You can get the x64 driver here:
http://www.cypress.com/?id=4&rID=48578
This is for all the old Evaluation Boards with the Cypress controller.