Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question.
Question:
In the analog Input specification of a differential ADC, what is the difference between Analog Input Voltage Range and Absolute Input Voltage?
Answer
A differential ADC has two input pins, Ain+ and Ain-. The analog value that the ADC will acquire and convert is the difference between these two input pins(Ain+ and Ain-) which means Ain+ - Ain-. The voltage range of this difference between Ain+ and Ain- is specified in the ADC specification table as Analog Input Voltage Range. Meanwhile the input voltage on a single ADC input pin is limited with respect to ground for both Ain+ and Ain- pins. The actual voltage that can be connected to each Ain+ and Ain- is found in the Absolute Input Voltage specification. For a unipolar pseudo Differential input ADC, the absolute input voltage and analog input voltage are equal, but for unipolar differential input ADC, analog input voltage can swing from -Vref to +Vref but the absolute input voltage is from 0 to Vref.