Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question

AD7606: FAQs

A common question on the AD7606 is what is the tolerance of the 1M ohm input impedance? This can become important when there is a high external resistance on the analog input, greater than 10k ohms for instance, or when a sensor with a high output impedance is used.

The 1M ohm input impedance of the AD7606 is a typical figure and can vary from part to part. For a typical production lot this can vary between 0.93M ohms and 1.02M ohms, at ambient temperature. A greater variation will be seen over the full temperature range from -40C to +85C.

It is also worth nothing that if an external resistor is needed it can introduce a gain error. It is recommended that a closely matched external resistor is applied on both Vx and VxGND to reduce any offset error. See the datasheet for more details. 

Comments
Anonymous
Related