FAQ
AD7112
Obsolete
The LOGDAC â„¢ AD7112 is a monolithic dual multiplying D/A converter featuring a wide dynamic range and excellent DAC-to-DAC matching. Both DACs can attenuate...
Datasheet
AD7112 on Analog.com
AD7111
Not Recommended for New Designs
The LOGDACâ„¢ AD7111 / AD7111A are monolithic multiplying D/A converters featuring wide dynamic range in a small package. Both DACs can attenuate an analog...
Datasheet
AD7111 on Analog.com
AD7118
Obsolete
The LOGDAC® AD7118 is a CMOS multiplying D/A con-verter which attenuates an analog input signal over the range 0 to -85.5 dB in 1.5 dB steps. The analog...
AD7118 on Analog.com
ad7115
Production
ad7115 on Analog.com