Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question.
Question:
What is the data output coding format used in AD719x family?
Answer:
On the AD719x sigma delta ADCs, two different coding options exist unipolar and bipolar coding. Unipolar coding is used to represent positive voltages only, and bipolar coding can be used to represent both negative and positive differential voltages applied to the analog inputs of the ADC.
For the ADC operating in unipolar mode, the input range to the ADC is from 0V to Full scale, where the full scale value is equal to VREF/Gain (reference input voltage/ selected PGA gain). The output coding is straight binary which means that
When the ADC is operated In bipolar mode, the input range is from negative Full Scale to positive Full Scale where Full Scale is VREF/Gain (reference input voltage/selected PGA gain). The output coding for bipolar operation is offset binary with