Post Go back to editing

LTC2353-18 and DC2365A/DC890B eval boards: More than 32k samples

I am evaluating the LTC2353-18 ADC with the DC2365A/DC890B eval boards using the Pscope software. The number of samples that can be recorded is 32768. Is it possible to increase the number of samples per recording beyond this limit?

Thank you!

Best regards, Christian

Parents
  • It could be made to work but it would require writing some software on your part to control the sneaker port (an I2C to SPI interface used to program the ADC) of the DC2365A-C and then do the data capture. It would be much easier and faster to use the DC2542A because the code for the DC2542A is already written. The code unfortunately is not compatible with the DC2365A-C. Because the DC2542A was designed to be used with the SoCkit board it has no need for the sneaker port.

Reply
  • It could be made to work but it would require writing some software on your part to control the sneaker port (an I2C to SPI interface used to program the ADC) of the DC2365A-C and then do the data capture. It would be much easier and faster to use the DC2542A because the code for the DC2542A is already written. The code unfortunately is not compatible with the DC2365A-C. Because the DC2542A was designed to be used with the SoCkit board it has no need for the sneaker port.

Children
No Data