LTM2893
Production
The LTM2893 is a high speed isolated µModule (micromodule) SPI interface with ADC control signals. The LTM2893 is optimized for isolating 1Msps high resolution...
Datasheet
LTM2893 on Analog.com
AD7983
Production
The AD7983 is a 16-bit, successive approximation, analog-to-digital converter (ADC) that operates from a single power supply, VDD. It contains a low power...
Datasheet
AD7983 on Analog.com
Hello everyone
I want to use LTM2893 to isolate SPI I/F for AD7983, is AD7983 compatible with the LTM2893?
On the datasheet of LTM2893, It is mentioned LTM2893 is optimized for isolating 1Msps high resolution 18-bit SAR ADCs, but these are only some suited legacy LTC ADCs on datasheet.
Do you have any recommended legacy ADI ADCs which can work well with LTM2893?
Best ragards
QI