Hello everyone
I want to use LTM2893 to isolate SPI I/F for AD7983, is AD7983 compatible with the LTM2893?
On the datasheet of LTM2893, It is mentioned LTM2893 is optimized for isolating 1Msps high resolution 18-bit SAR ADCs, but these are only some suited legacy LTC ADCs on datasheet.
Do you have any recommended legacy ADI ADCs which can work well with LTM2893?
Best ragards
QI