Post Go back to editing

ADI 5962-9312601MXA (Base part#AD1671)- DAV pin is not working doing ADC continuous conversion

We have assembled one board and mounted 5962-9312601MXA (Base part#AD1671) with IC Base.

During the calibration, We are unable tune ADC offset and Gain. When we are feeding ADC input -4.99, offset should be tuned to 000h ~ 007h, But We are getting 1E3 and unable to bring to 000h.

Similarly For +4.99V ADC input, We are getting the FFFh at 3.5V ADC input itself. We have probed the Encoder and DAV pin.

Its seems DAV is coming as pulsed signal ( frequently high and low) when encoder enable. It seems ADC doing again and again the conversion. Please reference attached image reference DAV_Defect_1.jpeg.

Later we are replaced with new ICs and its working fine. We are able to tune the offset and gain. DAV pin also working fine wrt encoder. Attached DAV_working part.jpeg.

Based on that, We have concluded go ahead for assembly of another two boards. We have assembled. then we went particular ADC offset tuning. In this both board while first transaction DAV pin ( frequently high and low) when encoder enable.DAV_Defect_2.jpeg.

Please can some one help me on this. Thanks!

ADC Schematics

attachments.zip
Parents
  • Hi Gopi.m123,

       It looks interesting. You mentioned that after replacing with a new IC, the system works fine. We can say that your system and schematic is working fine. Although again the problem is seen again, you may check some of the connection on the IC and make sure they are well soldered. Do you have changes in the schematic of the new board?

    Regards,

    Jonathan

Reply
  • Hi Gopi.m123,

       It looks interesting. You mentioned that after replacing with a new IC, the system works fine. We can say that your system and schematic is working fine. Although again the problem is seen again, you may check some of the connection on the IC and make sure they are well soldered. Do you have changes in the schematic of the new board?

    Regards,

    Jonathan

Children
No Data